Other Parts Discussed in Thread: TLV62080
hi,
as output current is between 75mA and 350mA, tlv62565 will enter PFM in which output voltage is 0.9% higher than that of normal mode. it causes image performace issue. with 10uH inductor, tlv62565 works in normal mode always and the issue is disappeared. any risk for 10uH inductor? detailed test report is attached, pls kindly check it and give your comments.issue caused by TLV62565-PFM.pdf