Dear BMC team,
One customer reported below issues when experimenting bq24100EVM.
For his application, customer may connect battery to the ouput of bq24100 while no voltage is applied at input.
In such case, he measured high peak current taken from battery (up to 18A).
Can customer damage our device when power is applied at output with no power supply at input?
What is your recommendations to limit the peak current ?
Second concern from customer is about Vbat voltage when no battery is connected. He measured 4.3V (Vbat is blu plot). Is it normal behavior ?
thanks
Paul