Dear Specialists,
My customer is confirming TPS2379 circuit.
And he has questions about the result.
Could you please advise?
---questions from the customer---
I have confirmed the operation of IEEE 802.3af PoE (15.4 W) and IEEE 802.3 at PoE + (25.5 W) with TPS2379.
By adding external FET, I have also confirmed the operation of PoE++(4 pairs 60W)
(1) By adding external FEt, is it possible to use IEEE802.3bt with TPS2379?
(2) Or it is not supported some PD classes of IEEE 802.3bt, does it not work at all?
(3) In case of TPS2373-4 does it work both IEEE 802.3af PoE(15.4W)and IEEE 802.3at PoE+(25.5W).
The datasheet described it is possible to use IEEE802.3at, but not described about IEEE802.3af?
How about IEEE802.3af?
---
I appreciate your great help.
Best regards,
Shinichi