This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25940-Q1: surrounding component value

Genius 4850 points
Part Number: TPS25940-Q1
Other Parts Discussed in Thread: TPS25940

Could you please advise surrounding component value.

CIN,R2,R3,CdVdT,R6,R7,RILIM,RIMON,Cout

They conider to use TPS25940-Q1 at below condition.

Vin,Vout typ6.5V

V(OVP):8V

ILIMT:1.0A

They will use PGOOD as over current FLAG(1A).

When they detect over current FLAG,they will shutdown this part using with EN.

Please see attached.

TPS25940-Q1_20170616.pdf

Regards,