Hi, team.
My customers are considering TPS53014 under the following specifications.
Specification:12V_Input⇒0.9V/12.5A_Output
Since I have received a question about the description of the current limit setting of this product,please support.
<Background>
The current limit setting value is considered by referring to the description of data sheet p 8 "OVER CURRENT LIMIT".
Because there is a requirement that the customer wants to use the familiar product (externally attached FET) Ron is determined by a fixed value.
Therefore, I want to adjust the current limit value with Vtrip value.
<Question>
Could you tell me any of the following?
(If you have a disadvantage using resistance values other than those listed in Datasheet, please tell me, it will be helpful if you let me know the reason.)
・Calculation method of Vtirp described in Datasheet (calculation formula)
・Or, create a graph in Excel from "Table.2 OCL setup resister table" data,can we get an approximate expression from the graph and reply as Vtrip calculation formula?
・Is it possible to present data between 11 KΩ and 18 KΩ?(12 KΩ, 13 KΩ ...etc:1kΩ step)
Could you help me?
Best regards,
Masumi Sekiguchi