I could't got a voltage above 5V at PMID.
So I contacted and solved.
solved link : e2e.ti.com/.../616105
But the problem remains.
I can't charge in connect VBUS and about 5V.
Through the above process,
I can getting to 5.05V from PMID.
And than I write REG01[7] = 1 to reset.
0 1 2 3 4 5 6 7 8 9 a
37 1b 60 11 b2 9a 03 4b 00 10 23
Next I write REG01 = 0x2B to PMID output.
AND i write REG05 = 0x8A to Disable watchdog.
0 1 2 3 4 5 6 7 8 9 a
35 2b 60 11 b2 8a 03 4b c0 10 23
Next I connect VBUS with 5V(external voltage to charge).
0 1 2 3 4 5 6 7 8 9 a
35 2b 60 11 b2 8a 03 4b c0 00 23
result REG08[5:4] = 00 .....
Non-charged state.....
In this case how do I charge it?
PS.
OTG was pull-up (with SYS, 10kohm)
AND GND can be connected with a jumper.
We can't arbitrarily change the jumper in a real system.
If use OTG connect GND to problem solving, change the circuit??
(problem solving = I can chage and PMID output 5V More than.)