This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54560: Inverting Power Supply Circuit

Part Number: TPS54560

Dear All,

We have designed Inverting Power Supply Circuit using TPS54560. I need to get +18V and -18V 4Amps from 36V Vin. The circuit for +18VDC works as we expected, but for -18V we could not get 4Amps, the output voltage drops according to load. In addition to schematic we add 1uF ceramic cap between Vin(2) and GND(7) pins. Do you have any idea for the reason?

Schematics, layout and Webench output are given below. All components choosen according webench part list.

/cfs-file/__key/communityserver-discussions-components-files/196/EK_2D00_5_5F00_TPS54560_5F00_SS_5F00_SIM.pdf