Other Parts Discussed in Thread: LM5118
Tool/software: WEBENCH® Design Tools
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Muhammed,
Thank you for reaching out to TI with your question. Please note that you can use the quick-start calculator to check your design as well. This will check component values and loop stability. I would suggest inputting your design parameters and seeing how the design looks. This design is similar to the LM5118-EVM which can also be used as a reference.
Looking through your design I would recommend the following.
1. Select and inductor with a higher saturation current than 11A. Looking through your calculations the efficiency of the converter is assumed to be 100% where in real life efficiency will be lower resulting in an increased peak current of the inductor. Increasing the saturation rating will also give more margin for load transient conditions.
2. Note that the current limit of the device is going to be around 15A. The inductor current should be increased or the sense resistor should be changed accordingly.
3. Please lower R46 to ~7kOhm. This will increase the gain margin of the control loop when VIN =5V.
Please let me know if you have any questions.
Thanks,
Garrett
Thank you for your comments.
I have little confusion from your reply.
I think you have taken the efficiency as 100%, but If you see in the design calculation, i have considered only 80% efficiency.And as per my calculation the Peak inductor current or Maximum switching current for boost mode operation is coming 7.35A.By considering 30% margin, i have selected an inductor with a saturation current rating of 11A. Can you please check about this and help me to verify the selected inductor part is sufficient for this design. Since i am having PCB size concern, i have to select a small size inductor for this design.Also let me know how this inductor current rating will effect the over all operation if i am going ahead with the selected inductor(I sat = 11A).3515.Buck-Boost Regulator_LM5118_12V-3A.xlsx
Buck-Boost Regulator_12V-3A.xlsxThank you very much for helping me to find out the mistake. As per your recommendation i have changed the equation.
Now i am getting the Peak inductor current or Maximum switching current for boost mode operation is coming 10.38A,
I have selected an inductor of the part number (SRP1770TA-330M).
Please let me know this will fit for my requirement. Also please go through the attached design sheer for seeing the calculation as per the new inductor.
Muhammed,
It looks like that inductor will not have enough current rating. The saturation current of the inductor is 15A but the current limit is going to be around 15.88A (cell D114). It could be possible to select a lower inductance value (22uH, 15uH) and keep the design relatively the same while increasing the saturation current of the inductor. Please make sure that the selected inductor has a high saturation current rating then selected current limit.
Thanks,
Garrett