Other Parts Discussed in Thread: BQSTUDIO
Hi,
I'm working on a project with the BQ35100, the product will be produced in series. Now the comunications is done using the EV2300, the main problem is that when I program the IC FW through bqStudio the result is the corruption of the chip due to the bad srec file, and this is not more able to talk on the I2C bus. From what I understood, also reading this post, the problem is related to the fw version of the EV2300 (3.1c) and the only way to overcome this problem is to upgrade the EV2300 fw, is this correct?