This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Resister of TLC59108



We use 5LEDs and  place the resistors in series with the LEDs.

  Vf of LED is 2.8~3.1V.

Resistors are used to suppress heat generation.

Question 1.

Please tell us the resistance value.

Current is 18~20mA

Question 2.

Please tell us the variation of current at IC spec.

Question 3.

Maximum current of this IC is 120mA.

If derating of this IC is 80%, Can we use the above methods?

Question of TLC59108.pdf

Best regards,

Takahiro Nishizawa

  • Hi Takahiro-San,

    Please refer the below comments.

    Q1: May I know the LED supply, normally it makes sure ILED * R + VLED< LED supply.

    Q2: please refer the datasheet page 6.

    Q3: This is the constant current device. Could you explain the derating for the detail?

    Thanks!

    Summer