This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2376-H: Possible to design with TPS2376-H at Vin:24V?

Part Number: TPS2376-H

Hi,

Is it possible to design PoE stage with using TPS2376-H for Vin:24V and Poıt:12W?

The customer's schematic is attached. It confirmed that the IC fails when the customer try to implement the design on layout. 

Could you please advise on this?

Thanks,

Mete

POE_IN _ 08 - POE.pdf

  • Hi Meta,

    The PD is likely not being detected since the UVLO resistors (R241, R244, R248) in parallel with the detection resistor (R242) brings the total detection resistance to ~23.5kohms, below the 1% threshold specified on page 6: www.ti.com/.../tps2376-h.pdf

    Try increasing the UVLO resistors (R241, R244, R248) while maintaining your voltage division ratio for UVLO.

    Thanks,
    Thomas A.