This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40322: Loop stability verification

Part Number: TPS40322


power supply block with TPS40322 was designed in accordance to the Application Note as well as the Loop Stability calculator file.

PDFs are attached. Can we count on an stable operation with the chosen values of the components?

The targeted outputs are

 3.3V@36Amps(single-phase),

1.8V@16Amps(dual-phase),

1V@8Amps(dual-phase)

0.9V@24Amps(single-phase).TPS40KType III Loop Stability - 0V9.xlstps40322.pdfhttps://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/196/TPS40322.7z