Dear All,
I have a design question regarding powering up the BQ EVM.
Currently what i have is I have two connectors
Connector 1 - connecting vesnse0 to 16 (Cell VSENSE Connecting on J1 BQ76PL455 EVM)
Connector 2 - BAT0 and BAT16 to power the BQ IC
The procedure followed is connecting connector 2 first and then Connector 1. What i would like to know is do we really need to power the IC 1st and then the Vsense ? or can we just connect all the J1 pins on BQEVM and just use that connector for powering the BQ IC and VSENSE all in same time ?
Regards
Vikram Jain