I have three questions:
1. What are the absolute maximum ratings of these pins:
COMP1, COMP2
2. What are the functions of these pins:
SW1, SW2: the block diagram shows these only serving as ground reference for the high side driver. Is there no other functionality associated with these?
RAMP1, RAMP2, RES: what are the V/I characteristics of these pins in the on and off states? How fast do the switches operate?
(I see the voltage rating has been answered already, ref: https://e2e.ti.com/support/power_management/non-isolated_dcdc/f/196/t/262250 )
COMP1, COMP2: V_OH and V_OL are provided, but one must still guess at the output type. The ratings and compensation connection suggest an op-amp voltage output, which therefore cannot be connected to other loads. But this is contradicted by the recommended two-phase connection, where COMP pins are strapped together. Is it actually a transconductance amplifier? If so, why not use an R+C to GND for compensation? If an external error amplifier is used, what voltage range can the COMP pins be driven to?
3. I'm looking at an application for an inverting type output. I would like to use a Cuk converter, for reduced ripple, and LM25119 is presently selected for other channels in the same circuit, so it would be convenient to reuse. (Also, that there are very few offerings from any major manufacturers, including TI, for multi-phase, synchronous Cuk converter applications, but if you can recommend something more suitable, I would be interested.) From what I can see in the datasheet, this should be acceptable, but in lieu of answers to the above, I cannot be certain that the "diode emulation" function will work correctly, or that an external error amplifier can be used.
Thank you for your time,
Tim