This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65400: Could you kindly help to check the schematic of TPS65400 and give some suggestions about some issue?

Part Number: TPS65400


Dears:

Could you kindly help to check the schematic of TPS65400 and the file as blow:

TPS65400RGZ.PDF

And pls. check the below information:

1. Is it OK about the 4 EN PINs of TPS65400?

2. Is it OK about the pull-up power being VDDD about the control Pins SDA, SCL, RST_N of TPS65400?

Btw, PG_D0V85 is 2.97V, and control the EN2 Pin of TPS65400.

Thanks a lot!

Best Regards

Luck Wu

  • Hi,

    i have reviewed the schematic.

    1. 4 EN pins connectin is ok.

    2. VDDD pull up the SDA, SCL, RST_N pin is ok too.

  • Hi,

    Additional comments:

    1. C148, C151 value is too large, i believe 4.7nF is enough.

    2. C155, C156, C158, C159 value is also too large, for common application, 4.7nF is enough.

    3. recommend C140, C146, C154, C161 value is 22uF.

    Besides, you can refer the TPS65400 EVM user's guide which is a good design start point.

    http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=slvuac4&fileType=pdf

     

  • Hi Zhao:
    Thanks for your help and suggestions.
    We will check it.
    Thanks a lot!

    Best regards
    Luck Wu
  • Hi, Zhao

    Thanks for your kindly reply!

    For item 2 and 3,  we will follow your comments.

    As for item 1,  the value of C148 and C151 in our schematic is  based on TI's WEBENCH Designer.  In our design, the output 3 is D3V3@0.22A, and output 4 is D2V5@0.12A.  The current of both 2 outputs are very small. I guess your comments is based on the output current is 2A, right?

    I creat a design example of TPS65400 using WEBENCH Designer, I set the output 3 is D2V5@2A, and output 4 is D2V5@0.2A. In the design, the Cc of  COMP 3 is 1.2nF, and Cc of COMP 4 is 33nF. Different current will need different Cc, right?

    Do we need changed the Cc in our design?  Also, the compensation circuit is Cc combines with Rc. If we change the Cc, the Rc should also be changed accordingly, right?

    Thanks!

  • Hi, Sir

    Yes, my comments are based on output curent=2A.
    Generally speaking, if loop is stable @ CCM, the loop will be stable @PSM too.
    When Iout is small(0.12A or 0.22A), IC will work in PSM, i think when C148 =C151 =4.7nF, the loop will be stable too.

    Of course, i think the calculation of WEBENCH Designer is right too, but it is over design.
    when Cc=22nF or 33nF, i think the loop is also stable, but the bandwidth will be reduced.

    So Cc=22nF or 33nF or 4.7nF are all ok, selection is up to you .  
     
    You can keep Rc value, or set Rc same as EVM value(15.4kohm).

  • Hi, Zhao

    Thanks for your answer!

    Best Regards.