Here's the schematic I have so far:
The circuit's input is a 24V DC carrier with a 2.176 MHz frequency that needs to be filtered out. Steady state current is about 700mA when the supply has its load.
I need the inrush current to be at about 400 mA or less. However, the 0.1uF capacitor on the input of the LM317 is causing me to have about 1A of inrush current. Can I get away with removing this recommended component?