I have questions about TPS56C215.
Can you confirm the attached document?
1.In the datasheet p.18, Are Ip1 and Ip2 pull-up from Vin?
2.Is it possible to input 3.3 V of CMOS to EN pin without using dividing resistance between VIN to EN?
3.And is it better to change the level by OpenDrain?
Best regards,
Takahiro NishizawaTPS56C215.pdf