hi,
I used LM5085 for Battery Charger.The circuit input D21 is 40V/8A.The voltage of Battery is from 31V to 39V.And the current must be more than 1.5A.The following picture is my design.The current of this circuit is not meet the requirement.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
I used LM5085 for Battery Charger.The circuit input D21 is 40V/8A.The voltage of Battery is from 31V to 39V.And the current must be more than 1.5A.The following picture is my design.The current of this circuit is not meet the requirement.
Hello,
Thanks for the question about the LM5085. Under what conditions do you not get 1.5A output? Have you tried to disconnecting the circuit for CV/CC operation, Q45 and R132 and apply the load directly across the output, C85?
Terry
Hello,
Thank for your reply.I use LM5085 for battery charger.When the voltage of battery was 30V to 37V.The current out of LM5085 is only about 300mA.
Have you tried to disconnecting the circuit for CV/CC operation, Q45 and R132 and apply the load directly across the output, C85?