This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5085: lm5085

Part Number: LM5085

hi,

I used LM5085 for Battery Charger.The circuit input D21 is 40V/8A.The voltage of Battery is from 31V to 39V.And the current must be more  than 1.5A.The following picture is my design.The current of this circuit is not meet the requirement.