This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello TI,
we are using the LMR23630A to power a GSM module.
Our layer structure is as follows
Signal+GND pour
GND
VCC
Signal+GND pour
The datasheet mentions that when the vin source is more than 5cm away from the LMR23630A, bulk capacitance maybe required.
The Vin trace is 0.8mm wide and nearly 12cm long. This trace exists is the third plane (VCC) From here I use vias to connect to the top plane where the Vin is a polygon.
The 12cm trace has an inductance around 220nH from a web based calculator.
How do I decide if I really do need the bulk capacitance.
1. The module is supplied by an automotive battery, taking into account capacitance derating and safety, I think we need at least 50V rated capacitor. The biggest question I have is, can I go with aluminium electroytic capacitors or should I rather go for the polymer based ones (OSCON etc)
2. The bulk capacitance is not used for bypassing high frequency ripples. So should the common guideline of keeping the return loop path as short as possible apply for the bulk capacitance too? Or is it ok to position the bulk capacitance as the layout permits? Or should I stick to the EVM layout?
Hello Yang,
thank you very much for your input.
The maximum current in the worst case scenario that we have measured is 200mA at 12V. Assuming a temperature rise of 10 degrees, that's around 0.9mm How much wider do you recommend the trace be?
How do I determine how much DCR is required? I think we will also stick with electrolytic capacitor.
Please find below the layout for the 12V -> 3.8V LMR23630A. Here I'm using a Panasonic case G aluminium electrolyte Cap. Highlighted is the Vin polygon pour on the top plane as well as the 0.8mm trace on the inner layer.
Is there anything more I can optimize with regard to the input capacitors? If the return path for the current through the electrolytic capacitor is not as critical as that for the ceramic bypass capacitor then I can leave the cap as it is.
For reference we use the following stackup
Layer 1 Signal + GND pour (red here)
Layer 2 GND
Layer 3 VCC shown in yellow, this layer is used to route Vin to both DC DC convertors on this board, as well as for the multiple voltages used by various ICs)
Layer 4 signal + GND pour (also used to route the feedback trace)
Thank you once again for the constant and really helpful support!