This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I could see a parameter called power good delay in TLV62568 datasheet.
Is this the time taken for Power good MOSFET to ON when output is 90% . If not, Can you tell me what is that means?
Regards
Anuraj NK
Hello Anuraj,
Thanks for your inquire.
You are correct. The power good delay is the time between the following events:
-Vfb falling from nominal value to the 90% of this one
-power good mosfet gets turned on
This delay can be measured between EN signal (high to low since it is Vfb falling) and PG pin (low to high) ?
Will probe the Enable pin and PG pin, measure the time interval from EN low to PG signal High.