Hi,
In my design, I need a current limit value of 400mA. Following the formula in the datasheet, RCL = (VCL(th) * K(CL)) / Iout, I need a RCL = 600 Ohms (see the design below). However, the current limitation is between 500-500mA on my 3 prototype PCB. This is over the rated ±15% accuracy in the datasheet. I am doing something wrong ?
Also, I have noticed this note for the Vcl(th) : Value specified by design, not subject to production test. What it is supposed to means? The value is subject to change between each IC ?
Thanks for your help, Mathieu.