Could you review above schematic, and please let me know whether there's any potential problem?
thanks,
TS
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Could you review above schematic, and please let me know whether there's any potential problem?
thanks,
TS
Hi steven,
thanks for your input.
1. What input voltage will be used? Is OVP not required (input FET is not blocking input adapter OVP)? What is the current limit for the input?
-> The input is connected to the adapter (5.0V/4A) through the eFUSE and into the Charger IC.
OVP is required. The OVP design is based on the "Typical Application Schematic with Single-Cell Unremovable Battery" in Datasheet.
-> The input current limit is not limited because there is no Rac Sensor resistance.
2. Which battery will be used? How much charge voltage is required? How much charge current is needed?
-> Battery is Max 4.2V CELL (see the attached file PM550-MZ952LI 规格 書 _A1_180117 (1) .pdf )
Charge Current is 1.5A.
PM550-MZ952LI 格 _A1_180117(1).pdf
3. What thermistor is being used? Make sure TS resistors are calculated properly.
-> see the attached datasheet below.
ECTH100505 103F 3830FST_AP(160819).pdf
For curiosity, what end equipment will use this charger?
-> End equipment is "Industrial PDA" and this charger will be applied in cradle.
I'll waiting your additional comments for this schematic.
thanks,
TS