Other Parts Discussed in Thread: TPS61220
Please let me know about two points below for TPS61291 operation;
【Condition】
・Vout: 3.3V
・EN/BYP pin:Held High level input (Boost mode)
・When Vin is 3.3V~3.78V, Vout occur large ripple. (Vout waveform is attached below)
・When Vin is more than 3.8V, Vout ripple was disappeared.
【Question】
①What TPS61291 operation in the condition of Vin≧Vout and Boost mode setting?
I want to know the reason of large ripple on Vin: 3.3V~3.78V.
②When Vin>3.8V, I think that TPS61291 changed Bypass mode, is it correct?
If correct, is there information for these operation?
Best regards,
Satoshi