This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM5576: Power Quick search recommendation to Webench Design simulation breakdown

Part Number: LM5576


Tool/software: WEBENCH® Design Tools

I filled out the Power Quick Search tool as shown below (attached Power Point). 3 recommended ICs are given, but only the LM5576 has a WEBENCH design associated with it. But when I try to open the Webench design, I get the error message “We're sorry, we could not find a solution to match these requirements. Please check to make sure your inputs are within the correct corresponding range.” The WEBENCH parameters were Vin Min 24.0 V, Vin Max 24.0 V, Vout1 -24.0 V, Iout1 1.2 A, and Ambient Temp 30 °C. Screenshots of the web pages are attached.  

Is there a reason for the breakdown between the Power Quick Search and Webench? 

Power Quick search  Webench Design breakdown.pptx