I did the following design :
when I connect the next solenoid:
Manufacturer Part Number -----> ROB-11015
V= 5V R dc= 4.5Ohm so the current should be ---->I= 1.11Amp
But the PMIC drop to 0V.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I did the following design :
when I connect the next solenoid:
Manufacturer Part Number -----> ROB-11015
V= 5V R dc= 4.5Ohm so the current should be ---->I= 1.11Amp
But the PMIC drop to 0V.
Hi David, this is the schematic and BOM:
I perform tests with a swiching source of 42V@ 2Amps.
BOM
| LM5085MY/NOPBCT-ND LM5085MY/NOPB IC REG CTRLR BUCK 8MSOP |
| ZXMP10A18KTCCT-ND ZXMP10A18KTC MOSFET P-CH 100V 3.8A DPAK |
| SRR1208-120MLCT-ND SRR1208-120ML FIXED IND 12UH 4.8A 25 MOHM SMD |
| 1655-1469-1-ND MBRD10200TR DIODE SCHOTTKY 200V DPAK |
| 399-15154-1-ND C1210C155K1RAC7800 CAP CER 1.5UF 100V X7R 1210 |
| 1276-2183-1-ND CL10C122JB8NFNC CAP CER 1200PF 50V C0G/NP0 0603 |
| 399-15154-1-ND C1210C155K1RAC7800 CAP CER 1.5UF 100V X7R 1210 |
| 478-3085-1-ND TPSB476K010R0250 CAP TANT 47UF 10% 10V SMD |
| 587-1282-1-ND EMK212B7474KD-T CAP CER 0.47UF 16V X7R 0805 |
| 311-1.82KHRCT-ND RC0603FR-071K82L RES SMD 1.82K OHM 1% 1/10W 0603 |
| 311-3.32KHRCT-ND RC0603FR-073K32L RES SMD 3.32K OHM 1% 1/10W 0603 |
| RR12P10.0KDCT-ND RR1220P-103-D RES SMD 10K OHM 0.5% 1/10W 0805 |
| CSR1206FK10L0CT-ND CSR1206FK10L0 RES 0.01 OHM 1% 1/2W 1206 |
| 311-68.1KHRCT-ND RC0603FR-0768K1L RES SMD 68.1K OHM 1% 1/10W 0603 |
| 490-11430-1-ND GRM1885C1E621JA01D CAP CER 620PF 25V C0G/NP0 0603 |
If you need I could upload the pcb.Thanks
Good morning David,
I implemented both suggestions and I obtein those results:
1) I place a series resistor with C30 and the value that I can use 42V was 1 Ohm. I could move the solenoid and its consume 10W....but the ripple is too big.
With 500mOhm doesn't work.
2) Doesn't work. The R41 is funtion that the times of PFET and obtein Noise in Vout.
Any other advice for improve Vout . thanks David
Hello,
1/0.5 ohms is too large. Can you try 50mR please?
If it still does not work can you show me somce scope captures of Vout and Switch?
Thanks.
David.
David,
I place and take scope's screen that you suggest.
and
While with 1 Omh the ripple at the output is almost 1V the signal SW is stable, while that does not happen with 30mR.
I hope it is useful, thanks David
Hi,
I had to travel and leave the project for a few weeks.
I tell you yesterday and today resume the tests. Because I do not have a wide availability of components, I told you what I was doing.
The output capacitor (Cout) is not low ESR, it has 250m.
TPSB476K010R0250
CAP TANT 47UF 10% 10V SMD
It is the one that recommends webench.
1) At the output I put in series 30m resistor. But when I placed the 5V load it fell to 3v.
2) Change Cout for 100uF of Aluminum. It generated noise.
3) Change the topology to get less ripple. I did not get good results.
4) Place a trimmer in Rt and probe with 68.5k - 70k - 90.9k - 243k and did not get good results.
I attach the webench report and the component list. The main components (L, D, Cout, Ic,Rsen) are the same.
I will attach the layout. Thanks
I resolved the problem.
Parts:
The inductive load mentionated in the first post was always the load.
steps:
I modified the Cfb for obtein a more representative Vfb. 620pF to 1200pf. This inside directly in the equation:
Cff = (3 * ton) / (Rfb1 // Rfb2)
Another change was the Radj:
1.82k to 2.2k
Icl = 40uA * (Radj / Rsen)
Thanks for the assistance and I hope it will be useful.