This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50EVM-561: BQ40Z50EVM-561

Part Number: BQ40Z50EVM-561
Other Parts Discussed in Thread: EV2400, BQSTUDIO

I am using BQ40Z50EVM-561 to evaluate LiPFO (2S2P) battery configuration,  planning to use bq40ia z50-r1 fuel gauge for application.

using ev2400 to communicate to PC via USB cable and SMB to  EVM560.

Three Leds ( USB, COMM, VOLTEN) are lighten on the EV2400.

2S2P connect to Cell1 and Cell2, and Cell3 and 4 will be shorted to Cell2+ as suggested.

Press S1 (Wake) and measure Voltage between, 1N and PACK+ register 6.66 VDC ( 2 cells )

Is there a trouble shooting guide for this bq40z50EVM-560? or any suggest to get pass this initial step to a quick start?

Activate Battery Management SW,  chose  Guage then device "bq40z50r1" the following come back

Download the latest driver for EV2400 and support component from TI website.

Error: NO ACKNOWLEDGE FROM DEVICE ( not seeing EV2400 communication)