Part Number: UC3710
Hi all!
I have some follow up questions on the UC3710DW:
Why is the lower temperature set at 0°C? Is it because the part has not been tested for negative temperatures or is it because it failed while tested at negative temperatures? Same question for the limitation at 70°C.
I am sorry to insist but can you propose a version of UC3710DW screened at -40°C to 125°C? I guess the answer to my previous questions will answer this one also.
Do you have any other bipolar based gate driver which are RoHS and have higher temperature ratings?
Thanks and Regards,
Annaïs