A question regarding the CHEM ID which is only accessible via a read-only command.
The Chem ID is not listed as one of the DATA FLASH (DF) parameters. Consequently, when a new DF file (file.gg.csv) is loaded, the CHEM ID doesn't get loaded.
Is the CHEM_ID value used as part of the impedance tracking algorithm? Does it have to be correct in order for the impedance tracking to operate from a different DF set?