Part Number: BQ25895
Hi
I have used the bq25895 in my design and I can only get 1.5A on the PMID pin with my battery connected, why is this? I added the VSKY20301608-G4-08 diode its a 2A rated, why cant even get 2.1A? But when I connect a supply to VBUS I get 3A+ on PMID. So I connected my power supply on the BAT connections and I still cannot get more than 1.5A!