Hello,
I have an application where I want to use the LM5066 so help with soft starting or current limiting the primary input capacitors into my design. I will have approximately 20mF of capacitance which the LM5066 needs to charge up to 24V.
At the moment the MOSFET I had planned on using is the SUM70060E.
Adding mutliple MOSFETs in parallel off of the same controller will not aid in SOA issues as one device will pick up most of the load until they are both fully on. So my question is if two LM5066 each with their own MOSFETs and sense resistors can be used together to charge the same cap bank from the same input supply.
Thanks!