Other Parts Discussed in Thread: BQSTUDIO
Tool/software: WEBENCH® Design Tools
Hello everyone,
I am testing battery of type : Lead acid , 12v ,1.3 Ah capacity.
Iam able to get voltage of 12v in bqstudio. To get the remaining parameters , i started performing learning cycle.
i updated the chem id to 0802, design capacity :1300 Mah , design energy :15600
Enable IT
2. Send Reset command (0x0041)
3. Charge the pack to charge termination.
4. Rest until the OCVTAKEN flag sets
5. C/7 Discharge to the termination voltage
6. Rest until the OCVTAKEN flag sets. At this point, QMax should update and the Update Status should increment to 0x05
7. Charge the pack to charge termination
8. Rest until OCVTAKEN flag sets
9. C/7 Discharge to the termination voltage
10. Rest until the OCVTAKEN flag sets. At this point, the Ra table should update and Update Status should increment to 0x06.
Should i charge with any current . i have charger with 15v ,1.1 A .. can i use it for charging the battery ... what values should i update to bqstudio for learning cycle...
Note:.Please consider i have very least experience regarding battery management.. please hele out me to complete learning cycle.