This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC256302: UCC256302 for an output power of 2KW

Part Number: UCC256302
Other Parts Discussed in Thread: UCC27714

Hi,

In reply to this thread:e2e.ti.com/.../681787

Ti is suggesting to go with the external gate driver for UCC256302 for an output power of 2KW with SW node connected to the HS pin for slew detection.

If I connect the HS to switch node,HO pin which connected to the External gate driver input will have (Vsw +VHB) potential w.r.t to ground.This would damage the external gate driver.

Can anyone suggest suitable circuit to use UCC256302 with an external gate driver.

Thanks,

Selvam.