This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EM1402EVM: J1 issue schematic

Part Number: EM1402EVM


Dear Sir/Madam:

Following the TIDM-TMS57004 Reference Design, battery connections according to the reference design on that reference design's webpage are through j1 which has 20 connections (Please see schematic from webpage). However the TIDA-00817 reference design has only 2 connections (Please see schematic from webpage). 

Issues

If possible please redirect to the correct schematic and mention the right battery connections and whether lead acid battery can be used fro 12 V?