Other Parts Discussed in Thread: TPS2490,
Hello,
I was reading the TI app note SLUA500 which shows a fast external turn-off circuit using the TPS2490 hotswap controller.
The recommended circuit for increasing turn-off speed in the LM5069 datasheet when using dv/dt slew rate for slow turn-on only removes the extra external capacitor; the turn-off speed is still limited to the current sink capability of the IC (which is pretty weak). The advantage of the circuit above for the TPS2490 is it uses the external transistor path to provide a stronger turn-off current than the IC can provide.
So my question is: is there any issue implementing the faster turn-off circuit from the TPS2490 app sheet with the LM5069 hotswap controller? I've simulated it and it appears to function as I would expect (slow turn-on, fast turn-off), but I want to make sure there are no gotchas before proceeding down this path.
Thank you,
Jessica