This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM46001: Lead Acid Battery Charger

Part Number: LM46001


   I will design the output 12 and 28V.

  The input voltage is input 18v at output 12v / input voltage is input 35v at output 28v

   I want to ask

   1. an the above circuit be used in lead-acid battery circuit?

   2. Can r5 in the above circuit change the output voltage?

   3. Can r2 and r3 in the above circuit change the output current?

* Output is always higher than input(I will design the input accordingly)
curious about the question below.
1. an the above circuit be used in lead-acid battery circuit?
2. Can r5 in the above circuit change the output voltage?
3. Can r2 and r3 in the above circuit change the output current?