This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: Configuration of multiple batteries after the "golden image" is created

Part Number: BQ78350-R1


Hi,

Let's say for instance I calibrate a battery (temperature, voltage, current, current offset), change all the settings and protections for the battery to the way I want it, acquire and load the data for the CEDV config and Chem ID and basically create the "perfect" battery... fully functional, just the way I want it. Then let's say I wanted to make a second battery just like it and decided to install the .srec of the first on to the second battery.

Question:

Besides non-essential settings like serial number, what would is everything that I need to do to this second battery for it to function as perfectly as the first?

Thanks,

JP