This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25088: LM25088 question

Part Number: LM25088

Dear TI community,

I've got a problem with the TI LM25088.

I had tried to set Vout as 4.2 V, Rfb1=1.6 kOhm, Rfb2=3.9 kOhm or Rfb1=2.2 kOhm, Rfb2=5.6 kOhm. but it is strongly depends on Vin and sets from 6.2 to 10.6 Volts. BTW if i put Rfb2  more greater then above Vout don't increases by more then 1 Volt.