This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92692: Wide Dimming Request

Part Number: TPS92692
Other Parts Discussed in Thread: TPS92691

Dear Sir/Ms.

My customer product spec. as following.

1. Vin : 12V ~ 24V

2. Vout max : 65V

3. Iout Max : 750mA

4. Support Analog and PWM dimming 

5. Output current can low to 1mA when use analog or PWM dimming

6. PWM dimming frequency as high as possible

Output current must from 1mA~750mA. Their previous product output current not linear from 1mA~25mA.

Did TPS92692 output current linear form 1mA~25mA when analog/PWM dimming?

Did TPS92692 support PWM dimming frequency at 25Khz?

Would you please give us some advice?

Best Regards,

Kami Huang