This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TINA-TI or Spice Models
FW a new high current DC- DC power convertor - TPS40428.msg
Hi TI Expert
we are looking for a new power DC- DC power convertor, for the application of tps40428, I have some question need you help:
1. For TPS40428, what the maximum current each phase can support, 25A or 30A? on page 1 main description, TPS40428 can support 4 phase to 120A, which mean 1 phase can support 30A, However, on page 78/79, test waveform and data only show 25A, which one is correct?
2. On page 7, the output overcurrent fault as below picture showing, which is for 1 phase output, right?
3. As you know, TI WEBENCH@Designer tools recommend TPS40428+ 2pcs CSD95378BQ5M (Mosfet),
CSD95378BQ5M’s VDD and Enable voltage range is 4.5 ~ 5.5V, However, no 5V output voltage on my board,
so can we divider 12V Vcc to 5V to it, do you think it’s ok?
4. Below picture show the main power dissipation, seems 2pcs mosfet’s power dissipation is up to 4.6W, need we add another heat-sink?
junction-to case thermal resistance is about 15C/W and junction-to board thermal resistance is about 1.5C/W,
which one is main for this type Mosfet?
5. Is TPS40428 in MP? Is there any critical issue when other customer use this part
6. How about the draft cost and lead time, it’s better for me is you can recommend us other good solution.
Best Regards,
Bruce Lin
Hi Bruce,
The OC fault limit is 40A (inductor peak current) per phase in factory default, and it can be changed to 50A per phase by PMBus.
For 2phase 70A design, the concern is power stage (CSD95378B) thermal. If the ambient temperrature is high, the power stage will be hot.
The power stage uses its power pad for heat dissipation, adding headsink on its top case does not help much.
I sugest you to use EVM to do some test. If the test result show power stage temperature looks fine, it should be ok to go with 2phase for 70A design.
Also, TPS40428 BP5 can not be used for power stage VDD (5V), because BP5 sourcing capability is not large enough. A small LDO is suggest to converter 12V to 5V for power stage VDD.
Thanks
Qian
Hi Bruce,
TPS40428 obtains the temperature signal from power stage TAO pin.
The temperature readout in PMBus is power stage junction temperature.
Thanks
Qian