Hello,
following the procedure in a post above, I have done the folowing to prepare the golden file:
- Found a good ChemID match for the new cells, by the use of GPCCHEM tool to find the a match.
- Export a gg file from the pack. Set the Update Status and both Cycle Counts to 0. Update the Design Capacity parameter.
- Program the default srec into the device.
- Program the updated gg file into the device.
- Program the ChemID.
- Calibrate the pack .
- Enable IT.
- Run the optimization cycle.
You can now create the golden pack.
- Export a gg file from the pack. Set the Update Status to 2 and both Cycle Counts to 0.
- Program the default srec into the device.
- Program the ChemID
- Program .the updated gg file into the device.
- Export the golden srec file.
Then, I upload the golden.srec into the BQ28Z610 installed in the new boards, test the boards and then we attach the cell and put into final enclosure.
We use the calibration data of the golden file, knowing they are not accurate like a calibration of each BQ, but it should be enough accurate for our scope.
What is the correct procedure after that? Is it necessary a further learning cycle or what kind of cycle has to be done to assure the FFC is in line with the real Capacity?
I supposed that discharge to empty and then charge to full would update the FCC at rated capacity, at least, but it is not so, only few batteries show FCC = or > than Desing capacity.
Thanks for your sugggestions ..
Maurizio