I use the LM34927 to converter 24V to 12V to drive the 16pcs relays. The relay core resistance value is 240Ω. So the output current of 12V about need to 711mA. And I check the datasheet of the LM34927 in page6 has the current minimum limit is 0.7A. So I want to ask below the two questions.
1. Can I use the LM34927 to converter the 24V to 12V to drive the 16pcs realys about 700mA?
2. If question 1 answer is Yes, how to decide the output inductor value, does it have any limit?