This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS82130: Inverting power supply

Guru 16770 points
Part Number: TPS82130


Hi

We want to generate -2V/1.5A output from 5V input.

Is it correct to calculate Vout  using normal equation as 0.8V * (1+R1/R2)?

http://www.ti.com/lit/ug/tidud32/tidud32.pdf

So is it OK to simulate in Webech with 2 V / 1.5 A output setting instead of -2 V output?

BestRegards