This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a question about TPS54550.
In datasheet, we can find the variation data of Vref when junction temperature is -40 to 125℃.
Min : 0.882
Typ : 0.891
Max : 0.899
Please tell us the variation of Vref when junction temperature is -10 to 70℃.
Max:
Typ:
Min:
Best regards,
Takahiro Nishizawa