Hello.
My customer is currently in use TPS54550, I have gotten a question about this product .
So , I have a question about TPS54550.
<Question>
Q1:Does this device will be able to use the Switching Frequency at 500kHz?
Q2:And , do you why that can be used the case of a Yes?
Because…
Download the Switcher Pro, was to operate the TPS54550 under the following conditions ,
the setting of "Switching Frequency" had become a 500KHz (RT = OPEN).
Use of the data sheet p13 Fig8 ~ 11 "Switching Frequency" in 500KHz is assumed to NG , but in this software you receive so no problem .
< Condition >
VIN: 11.64V ~ 12.36V
VOUT: 1.375V
IOUT: 5.0A
Could you help us?
Best Regards,
Pokkun