At www.ti.com/.../sluub41.pdf
bq76920, bq76930, bq76940 AFE FAQ
9.5 Is it okay to balance adjacent cells?
If 2 adjacent cells are balanced, the VCx pin between the cells does not change significantly in voltage. The differential input voltage of the next cell effectively doubles.
==>What is the meaning?
As described at 9.5:
As an example, assume all cells are at 4 V. If cells 4 and 5 are balanced, the VC3 input pulls to VC4,
which is approximately the cell 4 voltage or 16 V.
VC0--(cell 1)--VC1--(cell 2)--VC2--(cell 3)--VC3--(cell 4)--VC4--(cell 5)--VC5
==>
VC3, VC4, VC5 at the same voltage?
what is the voltage of VC0, VC1, VC2, VC3, VC4, VC5 when cell4, cell5 are balanced?
How come VC3 input pulls to VC4? VC4 input pulls to VC3???
VSS-VC0 above the absolute maximum is 3.6V? Does it mean that cell 1 cannot be balanced? because that VC0 pulls to the cell 1 value of 4 V?
Thanks