This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM503​​0: Usage of COMP and VFB pins

Part Number: LM5030

Hi, I'm Andy.

我想請問Lm5030是否可做初級側控制,通過VFB??

Does LM5030 Primary Side Control as PUSH-PULL topology by Vfb?

Thanks

PPD - [AUX-LVLM].pdf

  • Hello Andy,
    VFB is connected to ground in this circuit so the LM5030 is always operating at a fixed maximum duty cycle.
    There are 6 separate push-pull outputs and these are all controlled by linear regulators (U305,U302,U303,U307, U306,U304) on the secondary windings
    Regards
    John
  • Hi John
    Could I contol this topology by Vfb?
    It will contol in Vfb loop as Primary Side.
    Dose it work?

    Andy
  • Hi Andy,
    You can use the VFB pin to control variations in the input voltage (primary side).
    This is sometimes called line feedforward.
    This may give you acceptable line input regulation but you have 6 separate output voltage rails and you will still need the linear regulators on the outputs for acceptable values of output voltages.
    You need to specify:
    (1) Vin(min) and Vin(max)
    (2) Vo1(min) to Vo6(min) and V01(max) to V06(max)
    (3) I01(min) to Io6(min) and Io1(max) to I06(max)

    You will find that it is very difficult to design a power supply with one switching regulator and six independent outputs.
    That is probably why your application has a free running PWM and 6 linear regulators
    Regards
    John
  • Hi Andy,
    It has been almost 4 weeks and I have not received any further communication. I will close this thread for now. If you have any further questions please open a new posting
    Regards
    John