This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The Vin is 5V.
The inductor I used was 4.7uH which I got from the datasheet.
The layout is a bit different, but I would think I would get the right current for a very short time (unitl the IC reaches a specific temperature.)
The resistors are placed closer to the IC than the layout suggests.