Dear all:
What is the maximum input current for the PG and STAT pin? I want to calculate the resistance I need to limit the current for an LED that has a forward voltage of 2.1V and needs 20mA.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all:
What is the maximum input current for the PG and STAT pin? I want to calculate the resistance I need to limit the current for an LED that has a forward voltage of 2.1V and needs 20mA.
Hi Oscar,
The maximum current for the STAT pin is 6 mA (Table 7.1 in the datasheet). As for the PG pin, a current just over 30 mA is a good value to design for. The PG pin is an active low power good indicator which outputs logic LOW to indicate a good input if (among other things) the input current limit is >30 mA (Sections 6 and 8.3.7.1 in the datasheet).
Best Regards,
Angelo Zhang
Applications Engineer | Battery Charging Products