Other Parts Discussed in Thread: TPS22917
Hi,
Can you please advise if this device fits my use case.
Power supply is 5V, max 100mA
My device needs capacitor storage, in case of sudden power-off.
I calculated that the capacitance has to be 3000uF; (sufficient to write critical data to flash)
Therefore, I will use the TPS22810 to limit the inrush current towards the power supply which cannot handle large inrush currents.
I calculated and simulated with tina a Ct of 2uF.
When the device is disconnected from the supply, the output voltage will gradually drop to 3V within 250ms.
I added a series resistor of 5 Ohm to limit max current to 1A to preserve Imax
2 questions:
when sudden power off; Vin = 0V and Vout is max 5V; can this harm the device?
when powering on: can the device handle the power dissipation?
Regards, Wim